Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
XCL206 Micro DC-DC Converter Slide 1

Welcome to the Torex XCL206 Micro DC/DC Converter with Built-in Inductor product training module. Details concerning the Torex XCL206 micro step-down DC/DC converter  will be explained in this module. Features of the XCL206 to be discussed are: the ability to use the device much like an LDO but with greater efficiency and heat management; the space saving design and unique structure of the XCL206 which reduces the amount of radiated noise; and how low voltage ripple through the full range of load currents is a benefit of the technology employed by Torex.

PTM Veröffentlicht am: