Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
NFC Link Part 1 Slide 5

It was mentioned earlier that the current functionality of the NFC stack is implemented as a Windows GUI application. However, for an actual application, there are other options. It can be compiled as a driver component into the Operating System, or it can be compiled into an NFC module, where the NFC controller and NFC host are both on a dedicated CPU running full or parts of the protocol stack. It can also be compiled to run as a graphical user interface running on different Operating Systems including Windows.

PTM Veröffentlicht am: