Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
NFC Link Part 1 Slide 4

The NFCStack Evaluation application demonstrates the functionality of the NFC stack, which handles the higher layers of all three NFC operating modes after the anti-collision process. It has been developed based on the NFC Controller Interface (NCI) protocol from the NFC Forum to communicate with the NFC Controller to enable/disable the NFC operating modes. There are four tag platforms types supported, including Type 2, Type 3, Type 4A/B, and Type 5.

PTM Veröffentlicht am: