Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Topic 8 ControlSUITE Slide 21

In addition to USB, Concerto devices bring another new high value serial peripheral to the C2000 family with the introduction of an Ethernet MAC. ControlSUITE brings along the associated software to ease customer integration of this complex peripheral into the end application. The software solution for Ethernet actually looks very similar to USB in that it consists of three main pieces: application code, a protocol stack, and a driver library. TI provides several example applications on the next slide. TI also provides two TCPI stacks in ControlSUITE called lightweight IP and micro IP, both of these stacks maybe used in commercial applications for free.

PTM Veröffentlicht am: