Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Topic 8 ControlSUITE Slide 12

The Viterbi, Complex Math, and CRC Unit (VCU) adds a whole new realm of processing power to the Control subsystem and ControlSUITE adds a VCU support library to make it easy for customers to really make full use of the VCU. The library supports both real and complex FFT butterfly calculations, as well as 8, 16, and 32-bit single cycle per byte CRCs, and it also supports a two cycle Viterbi Butterfly. The API is extremely easy to use and TI has an excellent document that details the use of the whole library.

PTM Veröffentlicht am: