Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
VL6180X FlightSense Slide 8

The time required for the VL6180X to calculate an accurate distance is called the convergence time. The reflectance of the target material affects the convergence time. The reflectance reduces the number of reflected photons; therefore it takes a little longer to measure numbers of photons to make sure there is an accurate distance measurement. This graph shows that with a 3 % reflective target, at 10 centimeters, convergence time is below 10 milliseconds. With a white reflective target, the measurements are below 1 millisecond. Note: the numbers on the left side of the graph are in microseconds.

PTM Veröffentlicht am: