Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
VL6180X FlightSense Slide 7

The above graph shows the ranging performance of the VL6180X device, the y-axis shows the measured distance from the device and the x-axis shows the actual distance. The data shows a linear curve. There are four curves being plotted - a reflectance of 3 %, which is a flat black, a reflectance of 5 %, which is close to black, a reflectance of 17 %, which is medium gray, and then a reflectance of 88 % which is similar to a white piece of paper in reflectance. The graph shows that the travel time is not affected by the target reflectance.

PTM Veröffentlicht am: