Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
prod hi compar
This slide highlights the comparators, which also have a couple of families to highlight. The TS88 series is a low powered, nano-power comparator family which operates at 200 nA. The TS985 is one of the smallest comparators with a package size of approximately 1 mm². There are also high efficiency comparator families in the 16 volt group which are available in small packages.
PTM Veröffentlicht am: