Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
prod hi opamp
The TSZ12 series is a 1.8 V, low drift relative to temperature family. As the temperature changes there will be an increase of 30 nV/°C. Another component on this slide to highlight is the TSZ182, which is a combination of a low drift and a high speed, 3 MHz/1 mA amplifier.
PTM Veröffentlicht am: