Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
RF Reed Relays Presentation Part 1 Slide 22

The impedance is given by the mathematical equation: Z = √(R²+ (XL - Xc)² ) where XL and XC are defined by XL = 2πƒL and Xc = 1/(2πƒC); XL is the inductive reactance in Ω, Xc is the capacitive reactance in Ω, R is the DC resistance in Ω, Z is the impedance in Ω, ƒ is the frequency, L is the Inductance, and C is the capacitance. In this case R is the DC resistance of the signal going though the relay; XL is the inductive reactance generated from the inductance in the signal path; and Xc is the capacitive reactance generated from the capacitance which is made up of the physical characteristics of the reed blades and the shield running down the internal length of the relay.

PTM Veröffentlicht am: