Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
RF Reed Relays Presentation Part 1 Slide 2

First, it is helpful to understand where RF is used. Before the advent of the cell phone, RF was mainly used in radio transmitters and receivers, radar tracking systems, and an assortment of test equipment to support these applications. Now RF is used extensively in all cellular phones where the frequencies have climbed from 500 MHz to up over 4 GHz. These phones are filled with RF components that all need to be tested. This has given rise to a large number of RF testers coming into the marketplace.

PTM Veröffentlicht am: