Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
LDO Reg
This chart compares the power consumption of the C8051F900, with the integrated LDO, with a competing low power MCU. The core voltage of the C8051F9xx is a constant 1.8V and the core current is a constant 160uA / MHz, regardless of the operating voltage. This is reduced from 170uA / MHz and is still lower than the competition. Because power is the product of voltage and current, the power savings are exponential.
PTM Veröffentlicht am: