Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
CP2130-Slide10

In addition to the CP2130, Silicon Labs has several new exciting additions to the CP210x USB-to-UART family. First, consider the CP2104 Mini Evaluation Kit. The CP2104 Mini EK is a low-cost, small form factor evaluation board that can plug directly into a prototyping area on a development board or be used stand alone with jumper wires. It has a mini-USB connector and access to all pins via headers and test points. The kit includes the CP2104 mini evaluation board, mini USB cable and CP2104 quick start card. A leaded version is also available for the CP210x family as well. The CP2104 will be available in an SOIC-16 package and will be the first leaded package offering for the CP21xx smart interface products. Additional CP21xx devices are available in the SOIC-16 packages.

PTM Veröffentlicht am: