Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Functions Internal
The second control theme is the internal adjustment, or dial knob, of the box type controller. The PWM duty cycle is varied simply by adjusting the knob to the desired value, as shown on the printed scale. The PWM duty cycle follows a linear relationship with the 0 to 100% scale. This function is not found on the PCB type controller.
PTM Veröffentlicht am: