Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Wi-SUN Field Area Network (FAN) Module (cont’d.)

One advantage of the BP35C5 Wi-SUN module is that it allows users to create large scale networks because of its multi-hop function and the ability to connect to a maximum of 1,000 units, creating a mesh communication area. The automatic network repair function optimizes communication paths and recovers from communication failures. In addition, the BP35C5 Wi-SUN module does not depend on base stations and there are no monthly running costs.

PTM Veröffentlicht am: