Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Diode-Slide14

In general, Schottky Diode performance can be greatly affected by foreign particles that enter the device during the manufacturing process. Pn Diodes are not affected by particles because the P channel is protected by silicon. Schottky Diodes, on the other hand, are configured with the P channel very close to the surface, making them susceptible to foreign particles. In order to reduce the introduction of foreign particles and, consequently leakage current, ROHM has established IC-style clean rooms at all manufacturing facilities. The result is the lowest leakage levels in the industry and higher ESD resistance. ROHM Schottky Diode part numbers begin with the letters RB.

PTM Veröffentlicht am: