Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Advantage of Using GaN HEMT in an AC Adapter

One example of an advantage to using GaN HEMT devices is the reduction in the size of AC adapters. Since GaN HEMT devices can operate at much higher switching frequencies, this allows the magnetic components (e.g. transformers) being used to be smaller. In the example here, it is shown where the transformer size has reduced by approximately 1/2.5 times when switching frequency is increased from 100 kHz to 300 kHz. Moreover, since GaN HEMT devices can operate with much lower losses compared to silicon super junction MOSFETs, it is possible to have a solution that does not require any heatsink. This further allows miniaturization.

PTM Veröffentlicht am: