Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Slide24

To help illustrate the critical requirement for the on-ground (OG) antenna design to be physically taller, the electric field (E) simulated here shows most of the current energy is on the top of the antenna itself with very little of the energy forced onto the ground plane itself. The strongest field occurs across the top of the element itself. Since the ground return path is through the board, the effective distance from the underside of the antenna to the next ground layer will have the largest impact on the center frequency tuning of this antenna. It is for this reason all ground layers must be cleared out until the final ground pour on the bottom of the antenna.

PTM Veröffentlicht am: