Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Slide20

In addition to the benefits listed, there are also some challenges in applying a loaded PIFA. The PIFA is a unique antenna type. It is not commonly known and can not be treated the same in implementation as most of other antenna types (Patches, monopoles, and etc.) The antenna elements are connected to ground causing strong relation between antenna performance and PCB features. Because of this, the Board is part of the radiating structure; the whole board couples to body tissue in close proximity to the board. With the loaded PIFA, this coupling does not cause much detuning in frequency but degrades the total radiation efficiency. All electrically small antennas with ground connections suffer from the same effect to some degree.

PTM Veröffentlicht am: