Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
SP Caps Slide 8
These two curves are a comparison between the "SP-Cap" and an MLCC for capacitance change due to temperature and capacitance change with applied DC bias to the rated voltage of the capacitor. The MLCC’s capacitance decreases as temperature increases. Also the MLCC has a very large drop in capacitance as the applied DC voltage is increases in relationship with the capacitor rated voltage. The "SP-Cap" has an increase in capacitance with increases in temperature and no capacitance sensitivity to DC applied voltage.
PTM Veröffentlicht am: