Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
AN3018xA Series DC-DC Step-Down Regulators Slide 13
At the time of this presentation Panasonic has five products available. With two of the products users can control voltage through an I2C interface. For example, users can select LDO’s and DC-DC’s output voltage with 16 steps. As for the others, they can configure the output voltage through the external inputs. This series has max 3 MHz switching frequency, and so it contributes to downsizing the outer capacitor’s capacity and coils.
PTM Veröffentlicht am: