Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Dual Input vs. Single Input

The slide here shows how the NCP51561 can be configured as either a dual-input or single-input gate driver. On the left side of the screen, if pin 7 (the ANB input) is tied to ground, then OUTA equals INA and OUTB equals INB. On the right side of the screen, if pin 7 (the ANB input) is tied to VDD, then OUTA equals INA and OUTB equals the compliment of OUTA.

PTM Veröffentlicht am: