Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
summary
In summary, the LPC3250 is a microcontroller based on the ARM926EJ-S core. This device consists of the following modules: a CPU subsystem, a multi-layer AHB Bus Matrix, an on-chip memory, external memory interfaces, system functions, communication peripherals, and a variety of other peripherals. A variety of tools are available to aid in design and testing of a solution based on the LPC3250. NXP also provides a CDL that encapsulates the LPC3250 in many levels and includes support for several tool chains like GCC, Keil and IAR.
PTM Veröffentlicht am: