Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
stop mode
The STOP mode is the power saving mode of the LPC3250. In this mode, all CPU and AHB operations will cease and clocks are stopped to all peripherals except the USB block. The HIGHCORE output pin may be used to save additional power during STOP Mode or during low frequency operation like Direct RUN mode. It can be used to signal the external circuitry to lower the core supply voltage to 0.9V. This pin can be configured in software. Please note that the USB block will not be affected by the mode changes since it uses its own PLL.
PTM Veröffentlicht am: