Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
ir 85 150
In these graphs, measurements of the leakage current of a varistor and a Nexperia protection diode before an ESD strike, in black, and after the strike, in red, are displayed. It is clearly visible that at both ambient temperatures tested, 85°C and 150°C, the varistor shows a strong degradation whereas the Nexperia protection diode shows little or no degradation of the leakage current.
PTM Veröffentlicht am: