Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
protection cd
The capacitance of the protection device is an important parameter for protection of high speed datalines. The more capacitance present on the dataline, the more the signal is deteriorated; therefore, when the maximum allowed capacitance is exceeded, the functioning of the protected application is disturbed. The protection device is usually not the only capacitance on a dataline since the whole path on the PCB contributes to the capacitance. However, the less capacitance the protection device has, the less effort has to be spent to minimize the capacitance at other locations of the signal path.
PTM Veröffentlicht am: