Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Bridge Solutions Slide 21
Because of the hardware simplicity of the SPI interface and the ease of writing software, this bridge device offers many advantages over other solutions: Four wired host interface, fast SPI bus, there are only a few commands that need to be learned, Small 16 pin TSSOP package, and Five extra GPIO pins available for use.
PTM Veröffentlicht am: