Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Bridge Solutions Slide 13
This slide shows a typical use in the RS-485 network. The SC16IS7xx has built-in RS-485 automatic support; this feature reduces the frequency of false trigger interrupts the UART sends to the host. With other UART when there is traffic on the RS-485 bus the UART will capture the traffic data, generates an interrupt to the host even though the data are not sent to it. With the SC16IS750, the auto RS-485 allows the device to capture the traffic data only if the traffic is sent to it.
PTM Veröffentlicht am: