Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
SynJet® Thermal Solution
Pictured on this slide are the SynJet® ZFlow 75 and Spotlight Cooler 31 W Heatsink designed into a tracklight. The ZFlow 75 is comprised of two main assemblies: the SynJet FlexCool engine and the SynJet housing. The SynJet Flex Cool engine is used in multiple SynJet coolers. The type of housing determines which heatsink the SynJet cooler mates with, based on mechanical form factor.
PTM Veröffentlicht am: