Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List

7' BeagleBone Capes Slide 5

The 7.0” BeagleBone Capes are available in three different models featuring capacitive touch. Each touch version of the Cape is offered as either Newhaven Display’s standard, premium, or sunlight readable models. Depending on the user’s product needs, Newhaven Display’s 7.0” BeagleBone Cape line has a solution. If the product requires sunlight readability, the sunlight readable version will be the ideal choice. If the user needs wide viewing angles, the premium line features MVA technology enabling the displays to have up to 75° view from all sides. If they just need a TFT display that is affordable and looks good, then the standard will be the appropriate solution. Newhaven Display International’s 7.0” BeagleBone Cape product line has something for everyone.
PTM Veröffentlicht am: