Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Slide6

Engineered and assembled in Elgin, Illinois, USA, the 4.3” Arduino Shields are available in resistive or capacitive touch. Each touch version of the shield is offered as Newhaven Display’s standard, premium, or sunlight readable model. Depending on the user’s product needs, Newhaven Display’s 4.3” TFT line has the perfect solution. If the user’s product requires sunlight readability, the sunlight readable versions will be the ideal choice. If they need wide viewing angles, the Premium line features MVA technology enabling the displays to have up to 85o view from all sides. If the designer just needs a TFT display that is affordable and looks good, then the standard will be the solution. Newhaven Display International’s 4.3” Arduino Shield line has something for everyone and because the designer is developing with Newhaven’s 4.3” TFT display, they can easily go into production knowing that all of these shields feature a standard off-the-shelf product offered by Newhaven Display.

PTM Veröffentlicht am: