Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Image of MoSys Accelerator Bandwidth Engine: High Performance/High Bandwidth - BE2 and BE3

Shown here is the relative access performance of the most commonly available high-speed memories on the market. Those being QDR, Sigma Quad, and RLDRAM in relation to the Peraso bandwidth engine devices. From the horizontal axis it is seen that the actual access performance is tied to the pattern in which the memory is accessed. For example, if the Sigma Quad IVe is examined, the part was designed to take advantage of a balance read/write access pattern (or 50% reads and 50% writes). This is due to the bus structures on the device. This makes the device a good choice for a buffer application in which there is a temporary need to store data before sending to a “next” hop location. In this case an equal number of reads and writes will occur. Even under these circumstances, the Peraso devices out-perform Sigma Quad. Where Peraso shows an even greater differential is in a case where a larger percentage of accesses are reads (so table lookups and state memory type applications). Again, due to the device architecture and bus structures, a Peraso bandwidth engine device has its best access pattern at 75% reads and 25% writes. But even at 50/50, the architecture of the Peraso devices are one of the best options available.

PTM Veröffentlicht am: