Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Image of MoSys Accelerator Bandwidth Engine: High Performance/High Bandwidth - Bandwidth Engine 3

The bandwidth engine 3 (BE3) branch of the family is comprised of two devices (MSR630 and MSR830). The members in this branch are 1Gb in density and have options of either 12.5Gbps, 15Gbps, or 25Gbps interface speeds. These devices have been in production for more than 3 years and have a stellar record of reliability. In reviewing the main features of the BE3, it allows a user to perform up to 10 billion transactions per second, handle up to 32 simultaneous transactions per second which allows one device to support buffering or statistics for up to 400 GE. From the previously stated features of the BE3 device(s) it is possible to support types of applications like those mentioned in the chart in the lower right portion of the slide.

PTM Veröffentlicht am: