Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Product Highlights

After a general description, an in-depth look to the product highlights is worthwhile. InnoSenT strived to achieve the best results in design, performance, quality and price for the IMD-1100. The minimized profile of the product is certainly a benefit for integration – it fits optimally into most end-products. It is the smallest radar from InnoSenT and its size is comparable to a USB memory flash drive or cell-phone SIM card. The performance of the motion detector is unaffected by weather conditions and also can be used for indoor applications. Material, such as clothing of a person, does not hinder detection. Vandalism such as bubble gum stuck on the sensor or color sprayed on the covering will not cause any reduction in performance. Like all of InnoSenT’s products, the IMD-1100 is subjected to a rigorous quality control process. The company has years of experience in manufacturing, design and ESD packaging of sensitive components. The inexpensive radar front end is 100 percent end-of-line tested and is produced with modern production methods in compliance with the highest quality standards. Complementing the optimal price of the IMD-1100 and its positioning to meet low-budget motion detection applications, InnoSenT has made no concessions in quality and performance. The competitive price was achieved by optimized manufacturing processes. As a result of expertise in radar design and development, cost-reduction was possible. Compact size resulted in cost reductions due to less material demand.

PTM Veröffentlicht am: