Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
CBP-Slide5

Conformal coating is a process of applying a thin dielectric film onto a circuit board. Depending on the application requirements and the chemistry chosen, this coating could be applied between 1 and 10 mils thick. The coating is used to protect components and traces from corrosion, shorts, and mechanical damage. Conformal coatings are typically applied via spray, brushing, or dipping.

PTM Veröffentlicht am: