Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
CBP-Slide12

As there are multiple chemistry options, there are also multiple application methods. Dispensing is used for potting and gasketing applications. Whereas, spray, dip, and brush methods are typically used for conformal coatings. Low pressure molding is used for the Macromelt materials. Bergquist has the Loctite Equipment Engineering Group that uses partnerships with leading equipment manufacturers to provide equipment solutions.

PTM Veröffentlicht am: