Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
inverter-slide7

For the same circuit, these waveforms show the IGBT turn-on and diode turn-off with a Si and SiC diode. Note the elimination of the diode recovery current and the resulting decrease in the IGBT current and overshoot. Silicon Carbide produces a large reduction in area under the power curve (orange) showing the decrease in IGBT turn-on loss. 

PTM Veröffentlicht am: