Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
ip ratings
IP ratings are established by the International Electrotechnical Commission under IEC 60529. It was originally the standard used outside of North America, but now it can be found internationally as well. Much like with NEMA, the standard setting body does not actually do the testing; this is done by a separate approved certification laboratory. These ratings provide the criteria for evaluating an enclosure’s ability to protect against the intrusion of both particles and liquids.
PTM Veröffentlicht am: