Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
nema more
All of the testing processes are very specific. For example, to pass the NEMA 4X rating, the test utilizes a nozzle of 1” diameter delivering water at a pressure of 45 gallons per minute at a distance of between 10 and 12 feet. The spray must move along all joints at a rate of ¼ inch per second. No matter the rating, the tests are equally specific.
PTM Veröffentlicht am: