Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Basics of Wire and Cable Slide 22

There are many additional properties that can be considered in the selection of a jacket material. The application will dictate the need for some of these properties and not for others. It is vitally important to understand the advantages of the various materials used for insulation and jacketing to be able to find the correct solution.

PTM Veröffentlicht am: