Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Basics of Wire and Cable Slide 21

There is a lot of air in a semi-solid cable. A solid rod of insulation is spirally wound around the conductor to ensure proper spacing is maintained between the center conductor and the tube of the insulation that is extruded over both the conductor and the spiral wound insulator. It is used mostly in coax constructions where higher performing electrical characteristics are required. However, with the increase in popularity of twisted pair cables, the use of this cable type is decreasing.

PTM Veröffentlicht am: