Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
pushpin-slide8

ATS’ pushPIN™ compression springs add the necessary force to hold the assembly together for secure attachment. An integral spring on each pin provides approximately 2 lbs. of retention load, depending on the height of the component and the PCB thickness. An online tool can be used to guide the engineer for the automated selection of the proper pushPIN™ configuration suitable for the application at hand.

PTM Veröffentlicht am: