Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
VHB-Slide11

This next section will list typical applications in electronics for 3M VHB Tapes starting with the popular application of attaching the bezel to the display in a flat-panel monitor. The tape is applied along the entire perimeter of the bezel, and is then attached to the display. A continuous roll of tape may be cut to size during the production step and applied in place or may be pre-cut to the exact lengths to speed up the manufacturing step. This pre-cutting of tapes is performed through a die-cutting operation as described in the next slide.

PTM Veröffentlicht am: