Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
PSA101-Slide18

Temperature can also influence the performance of the pressure sensitive adhesive. Low temperatures can have a negative affect such as reduced adhesive tack and increase shock sensitivity. On the other hand, high temperatures can cause adhesive softening, reduce shear and cohesive strength. It is very important to know the temperature range of the application, then select an adhesive that will meet both the high and low temperature extremes.

PTM Veröffentlicht am: