Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
PSA101-Slide16

Finally, the third factor is application. It is important to consider time, temperature and pressure for a pressure sensitive adhesive. Acrylic pressure sensitive adhesives require a dwell time to flow out and achieve maximum peel strength. The surfaces should be at room temperature or above and only light contact pressure is required as long as air is not trapped in the interface (15 pounds per square inch for flexible to rigid and flexible to flexible for 5 seconds).

PTM Veröffentlicht am: