Maker.io main logo

The Chemistry of Heatsinks

176

2024-05-24 | By Andrew Chen

Heat Sinks

In this blog post, we will be going overheat sinks, the chemistry and science behind them, and why we use them in some electrical applications!

A major concern in a lot of electronics is excess heat energy as a result of electrical current flowing through our devices. You may have noticed that after using your laptop or your smartphone for a long time, your device might feel a little warm, and this can be due to a multitude of reasons: an overworked CPU, a strained battery, or more commonly, using the device for too long.

The Chemistry of Heatsinks

Generally speaking, your phone and/or laptop will be fine after cooling down without any permanent damage from the heat, as long as there isn't an extreme level of heat. However, with devices that are more sensitive to heat, this can be a major concern, especially if their performance gets dampened. For big CPUs, this excess heat can fry the internal components, which can seriously damage your computer.

Here's where heat sinks come in!

The Chemistry of Heatsinks

There are a couple of elements to consider for a great heat sink:

  • The choice of material for many heat sinks is usually a conductive metal, like aluminum or copper. This means that on a circuit board, heat will have a tendency to transfer from certain temperature-sensitive components to these heat sinks where these heat sinks are more readily equipped to dissipate high amounts of heat energy compared to an important IC.
  • Heat sinks generally have protruding "fins" which massively increase their surface area. This is a huge benefit because the increased surface area encourages a faster heat transfer (due to more contact) with the surrounding air around it. Combined with a fan that forces air onto the heat sink, your electronics can be better protected from being fried.
  • As heat is transferred to the heat sink, the air surrounding the heat sink becomes warm, forming a convection current that draws in cool air to take its place. This passively prevents the heat sink itself from getting too hot.
  • Lastly, thermal paste or a thermal pad may be used to better the connection between specific components and the heat sink itself. That way, heat has a direct path to dissipate directly to the heat sink and ensure quicker heat transfer.

The Chemistry of Heatsinks

So, where are some applications of heat sinks in our everyday world? In reality, they are so important that they are seen in almost any real-world application, from HVAC systems to heating and cooling systems in power plants and in many consumer electronics.

The Chemistry of Heatsinks

The Chemistry of Heatsinks

In summary, heat sinks are used to disperse heat in the system they are deployed in to improve performance, and reliability, and prevent premature failure of electronic devices, meaning that your devices can be less frequently replaced/fixed and will have a longer life span.

A quick example where a heat sink can be quickly applied is a simple voltage regulator; unlike buck converters, voltage regulators are notorious for dissipating a lot of heat, especially when there's a high voltage differential between the input voltage and the voltage rating of the regulator.

The Chemistry of Heatsinks

A quick solution to this would be to use a heat sink to help ensure the voltage regulator has a way of dissipating the heat. With just a few extra cents, the voltage regulator can last a lot longer and maintain a more constant performance throughout its lifetime.

That's all about heat sinks today! If you find this blog post informative, please share it with your friends!

Herst.-Teilenr. 507302B00000G
HEATSINK TO-220 2.5W LOW PROFILE
Boyd Laconia, LLC
Herst.-Teilenr. 576802B04000G
HEAT SINK VERT PLUG-IN TO-220
Boyd Laconia, LLC
Herst.-Teilenr. 574502B03300G
HEATSINK TO-220 VERT MNT W/TAB
Boyd Laconia, LLC
Herst.-Teilenr. MC7805ACTG
IC REG LINEAR 5V 1A TO220
onsemi
Herst.-Teilenr. SP400-0.007-00-54
THERM PAD 19.05MMX12.7MM GRAY
Bergquist
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.