Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
key tech1
What separates the Furuno GNSS receiver from the competitors is the use of various technologies. The GF-87 series GNSS receiver measures the transit time of signals sent by the GNSS satellites and calculates its position from the distances between the receiver and the satellites. When the GNSS receiver antenna is not directly receiving the satellite signals but instead reflections of these signals, a position error may occur since the computation of the distances between the receiver and the satellites may be biased. The use of the Advanced Multipath Mitigation function allows Furuno's GNSS receiver chips and modules to mitigate position errors caused by the reception of the reflected signals. The Advanced Multipath Mitigation function allows the receiver to directly distinguish received signals from reflected signals and processes them to compute accurate positions and provide precise ground tracking.
PTM Veröffentlicht am: