Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Applications

The ISOA series resistors are designed to be used in active discharge, passive discharge, and pre-charge circuits typically found in passenger and commercial electric vehicles. When used in active discharge applications the resistor’s temperature can be monitored directly while applying power, by using the optional NTC thermistor to maintain the resistor’s temperature below its maximum limit of +150°C. This allows for greater control of the discharge pulse.

PTM Veröffentlicht am: