Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
VCNL4035X01 Digital Gesture Sensor Slide 9

The VCNL4035X01 has higher sensitivity than the VCNL4020 or 4040. Previously the longer range was mentioned, the graph on this slide demonstrates that point. Using a Kodak gray card which has 18% reflection, it can be seen that for a particular emitter current the 4020 has a range of 30 mm, and the 4035 has a range of 100 mm. The VCNL4035X01 has three times the range.

PTM Veröffentlicht am: