Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
OCB100-KIT Auto-Calibration Design Kit Slide 14

To use the OPB885CZ sensor with an opaque target, adjust the phototransistor load resistance to 2.5 Kohm by placing the shorting bar on the board between pins 1 and 2 of the header. Insure that no object is blocking the sensor gap, and then initiate the calibrating process by momentarily grounding pin 4 of connector J1. After approximately 2-3 seconds a green LED should flash three times to indicate a successful calibration. There should now be no LEDs lit if the board calibrated successfully. If instead the red LED is on, change the load resistor to a larger value and repeat the calibration process.

PTM Veröffentlicht am: